Define Predicted Parameter

Predicted Parameters are defined with the template for specific asset or system. For Example, ‘Remaining Life of Asset’ or ‘Remaining Life of System’ is defined as predicted parameters and the values for the same will be mapped with an algorithm which will predict the remaining life of an asset or system.

Perform the following steps to define predicted parameters:

  1. Click Predicted tab in Parameter page.

    When adding a record for any parameter under the Parameter section (Constructional, Operational, Derived, Predicted, or Physical Property), if a parameter is already associated with any of these categories, it does not appear in the add record parameter list. For example, if you add a record for a Constructional parameter, the same parameter is not available for selection in Constructional or any other listed categories.

  2. Click Add Record button. Add Parameter tab opens and lists all the available parameters.

  3. Select the Predicted parameters needed for this template by selecting the check box next to the parameters.

    You can also search the required parameters using the search box in the top right corner of the window.

  4. Click Add.

  5. Click Save.

  6. Click Referencetab in Parameter page.

  7. Click Add Record button. Add Parameter tab opens and lists all the available parameters.